Good corrosion resistance is essential when using metal parts in aggressive environments. JW Winco therefore now offers even more standard parts in the higher quality Stainless Steel grade AISI 316L (A4). The Winco product range has always included many non-rusting standard parts. But not all stainless steels are the same. Roughly 120 types with different alloy compositions are listed in today’s material catalogs. While Winco has historically concentrated to date on use of the AISI 303 (A1) and AISI 304 (A2) grades because these can be machined more economically, the market leader in standard parts now also offers an entire range of products in the more resistant AISI 316L (A4) variation as well – especially for use in aggressive environments.
|