Cross spirit levels GN 2276 are used to check the horizontal position of jigs, machines, devices, appliances and instruments.
The spirit levels of type AV are aligned in relation to the reference surface so that the bubbles are centered in the middle of the marking lines once the horizontal position of the contact surface is reached.
The spirit levels of type JV are aligned using the mounting holes that are offset by 120°. An alignment ball on the bottom serves as a pivot point. With careful tightening, it is possible to achieve an alignment that places the bubbles between the middle marking lines.
This article is RoHS-compliant in application of Annex III., which means it complies with EU Directive 2011/65/EU, including extension (2015/863/EU), for restricting the use of certain hazardous substances in electrical and electronic devices. The Directive regulates the use of hazardous substances in devices and components. The implementation in national law is summarily described with RoHS(Restriction of (the use of certain) hazardous substances)).
Weight: 0.209 lbs
If weight is not listed, please contact our Sales Department for additional information regarding weight. Phone: 800-877-8351